JT part attribute CAD_DENSITY not mapping to JT_ASSOCIATIVE_BODY Solid Body Density
2021-10-06T23:27:44Z
Summary
Details
On importing .jt file in NX, which is having attribute "CAD_DENSITY", NX is not utilizing this attribute value to calculate the density of the imported solid body.
Solution
Utilizing the attributes from the *.JT files for calculating Density, mass etc is not supported in NX.
Utilizing the JT attributes for calculating Density and other properties is supported in Teamcenter Visualization.
Hardware/Software Configuration
Platform: INTEL OS: windows OS Version: 1064 Product: NX Application: NXMANAGER Version: V1899 Function: FILE_OPEN