Getting invalid file name error while cloning using ug_clone.exe

2021-10-06T23:27:44Z

Summary


Details

Getting invalid file name error while cloning using ug_clone.exe, for assemblies having part family members with using the "-fam" switch with "strip_status" value.

"%UGII_BASE_DIR%\NXBIN\ug_clone.exe" -o=clone -fam=strip_status -assembly=%clone_from% -default_action=clone -default_directory=%clone_to% -default_naming=name_rule -name_rule=append:" "

Solution

The -fam switch cannot have strip_status value for cloning in both native and managed NX clone utility ug_clone.
So instead use the value "loose' for such assemblies.

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1926
Function: CLONE

Ref: 002-8512474

KB Article ID# PL8512474

Contents

SummaryDetails

Associated Components