Error While saving assembly "The same title cannot be used on two different attributes".

2021-10-06T23:27:44Z

Summary


Details

Error While saving assembly "The same title cannot be used on two different attributes". 

The customer is facing a problem that unable to save NX data with an error.

"The same title cannot be used on two different attributes"


How to fix the issue?




Solution

Under View Section Dialog we have an option called Body Color. So, if you define different colors to your geometry then you can see these colors in the clip. Refer below snap for your reference.


As this is Part/Assembly specific issue so kindly try below and do let us know if that helps to resolve/fix the issue.
 
- Open the Assembly in Full Load condition (Switch off Partial Load option)
- Go to File > Utilities > Part Cleanup > Under Part Cleanup dialog use "Work part and Components under 'Part' drop-down > Select the appropriate options for cleanup, especially "Delete Invalid Part Attributes", like as below snap and save the assembly using Force Save All option (File > Save > Force Save All).
 
 


Notes and References

9825232



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CORRUPTED_PARTS
Version: V1915
Function: MODELING

Ref: 002-8512163

KB Article ID# PL8512163

Contents

SummaryDetails

Associated Components