Solid Edge Default values for 'maximum time' and 'number of iterations' in Solid Edge goal seek

2021-10-06T23:57:20Z
PART/SHEETMETAL

Summary


Details

A user uses goal seek to determine the fill level of containers. Since the containers are quite complicated, the default 'maximum time' of 60 seconds is usually not sufficient. The user wants to have another default value for the 'minimum time'.  Is there any way to define a new default setting?



Solution

Currently, there is no way to set another default than 60 seconds for 'maximum time'. 

Notes and References

Enhancement Request #9828472 requests this functionality.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V220MP8
Function: TOOLS

Ref: 001-9828472

KB Article ID# PL8511987

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN