SEEC format definition of SE Cut Length

2021-10-06T23:57:19Z

Summary


Details

Is there a way to configure or define the used format of the value of "SE Cut Length" that will be transferred into the BOMLine attribute (e.g. by SEEC Preferences or Solid Edge settings)? 

We are using Teamcenter and Solid Edge locale English (US) throughout all installations and the format is, as shown in this example, "1,800.00 mm" which is a mixture of non-metric notation consisting of "." and "," with a metric unit of measure. 



Solution

The format of the SE Cut Length is controlled by the Windows region settings of the SEEC client.  If you use a comma as the decimal separator in Windows it will be used by Solid Edge and therefore the SE Cut length will also have a comma as the decimal separator.

Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC

Ref: 002-8511886

KB Article ID# PL8511886

Contents

SummaryDetails

Associated Components