NX
Machine Code Simulation: Program name 'TO_INI' not found.
2021-10-06T23:27:44Z
NX for Manufacturing
Summary
Details
"Machine Code Based Simulation" reports "Program name TO_INI in not found" . "Manufacturing Machine Samples", using a "Sinumerik" controller..display the following alert...
Solution
The Post Configurator postprocessor must have the desired output handler for the TO_INI file. Select the following to set the outputfolder...
Selection of the desired "Outputfolder" will define how the INI file for the cse simulation should be handled.
Part The ini files are output to a subfolder \\cse_files\\subprog of cam part file location. If \\cse_files\\subprog does not exist, post creates this folder. (User must have write access to the location)
CSE The ini files are output to sub folder \\subprog of \\cse_driver folder, which is located in same directory of \postprocessor in the respective machine kit. (User must have write access to the location)
ENV The ini files are output to a sub folder \\subprog in a directory specified over the environment variable UGII_CAM_CSE_USER_DIR. (User must have write access to the location)
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: CAM Version: V1926 Function: ISV