Method to create an inter-part WAVE link in a mixed unit assembly

2021-10-06T23:27:44Z

Summary


Details

Need a workflow to wave link a body in an inch assembly into a mm component.



Solution

In order to overcome the mixed unit work/displayed part limitation for this case, create a new mm parent assembly above the existing one. You will then able to make the mm component the work part and link a body in from the inch component. Once the operation is complete you do not need to save the newly created temporary mm parent.

The reason this process is necessary is because NX requires the Work Part to be the same units as the Displayed Part. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V1899
Function: CONTEXT_CONTROL

Ref: 001-9830550

KB Article ID# PL8511564

Contents

SummaryDetails

Associated Components