File Properties Dialog window does not retain position

2021-10-06T23:57:19Z

Summary


Details

The File Properties Dialog is always positioned at the top left of Solid Edge and will not retain its position if moved and then closed at the new position. 

Is it possible to set a registry key to retain the last used position?



Solution

This is not possible for File Properties.  This dialog is an OS window and Microsoft does no–t support the repositioning and resizing of the windows.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V220MP8
Function: UI

Ref: 001-9820685

KB Article ID# PL8511461

Contents

SummaryDetails

Associated Components