Solid Edge How to run different versions of Solid Edge with one Node Locked License

2024-08-05T06:08:36Z
PART/SHEETMETAL SETUP

Summary


Details

In this example, a customer is currently using Solid Edge ST10, for which they have one Node Locked License.  However they would like to test Solid Edge 2020 in order to compare both versions.  Since the Node Locked License is tied to a specific machine, the customer they would like to know if there is a way round this.

Solution

The solution is to use Cloud Licensing.  By using this license, the customer can install Solid Edge 2020 on a new machine in addition to their existing ST10 machine.

The new machine has another Composite ID, which would normally require a separate license file.  However, when using the Node Locked License in the License Management Tool as a Cloud License by assigning a Webkey user to a non-assigned License, after that the customer can start the Solid Edge License Utility on either machine and click the option:

"I am Cloud enabled"

In that way a special License will automatically be created for that machine so that when starting Solid Edge, the customer is required to enter their Webkey and Password in order to use Solid Edge.

Notes

The user should not run both machines simultaneously as that could cause the Cloud license to lock up and then they will not be able to use their Webkey until it clears.

Notes

If you have further inquiries about Node Locked Licensing please refer to the FAQs collection link below:

Solid Edge Node Locked License FAQs Collection


KB Article ID# PL8511087

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES