NODE LOCKED in VMWARE

2024-08-05T06:13:40Z

Summary


Details

Customer wants run Solid Edge 2020 NodeLocked license in a VMWARE environment. Are there any known issues? 

Solution

To run a Solid Edge 2020 NodeLocked license in a VMWare environment you will need to have the license encrypted using the COMPOSITE2 value of the VMWare machine. You can capture the COMPOSITE2 value by running the Solid Edge 2020 License utility. The COMPOSITE2 value is displayed in the left center area of the Solid Edge 2020 license utility dialog. This is specific to having Solid Edge 2020 installed on the VMWare machine and licensed for that machine. It will behave the same as a standalone machine would. Keep in mind, remote desktop to the VMWare will not run Solid Edge as remote sessions are not supported on Solid Edge 2020 NodeLocked licenses.

Notes

If you have further inquiries about Node Locked Licensing please refer to the FAQs collection link below:

Solid Edge Node Locked License FAQs Collection


KB Article ID# PL8510947

Contents

SummaryDetails

Associated Components