NX Image is missing when publishing Work Instructions as PDF

2021-10-06T23:27:43Z
NX for Manufacturing

Summary


Details

When publishing Work Instructions to PDF, the images are missing in the created PDF file.

Solution

To be able to publish Work Instructions to PDF, an open source application called wkhtmltopdf has to be installed on the computer (in the default location C:\Program Files\wkhtmltopdf). However, the behavior has changed in version 0.12.6. It now disables local file access as default, which causes this problem with images.

https://stackoverflow.com/questions/62315246/wkhtmltopdf-0-12-6-warning-blocked-access-to-file

The workaround is to install wkhtmltopdf 0.12.5 instead.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V1899
Function: WORK_INSTRUCTN

Ref: 002-8510926

KB Article ID# PL8510926

Contents

SummaryDetails

Associated Components

Manufacturing General