Details
Alternate Position is not displayed correctly on Graphics in Teamcenter.
Solution
In TC\structure manager SE assembly display/orientation is not controlled by SEEC.
To overcome this issue define a model view in SEEC assembly and then upload it to TC.
Use that model view in TC\structure manager hide show panel (viewer) to visualize.
With this the display/orientation in structure manager will match with SEEC display.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC
Ref: 002-8510737