How to add pin hole symbol to engineering drawing?

2021-10-06T23:57:16Z

Summary


Details

How to add pin hole symbol to engineering drawing? 

Solution

The pin hole symbol is actually placed as a block in the default template. You can access it, place it, and scale it in a draft file.
 
Steps:
- In Draft file go to Library > Select 'Active Document' > Select 'COM' Block > Drag it to the drawing sheet graphics windows.
- There you can  place it, and scale it as per requirement.
- For Scale 1 the dimeter of the pin hole symbol is 10.00 mm for ISO Metric template.

Notes and References

9741636

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V220.0
Function: SYMBOL_LIBRARY

Ref: 002-8510731

KB Article ID# PL8510731

Contents

SummaryDetails

Associated Components