Surfaces are automatically hidden in top level assembly.

2021-10-06T23:57:15Z

Summary


Details

When opening an assembly with a surface part, the surface is hidden by default.
 
User want to see surface parts in assembly by default, instead of showing the surface manually.
Is there any method to change default of Assembly display?

Solution

User can show the surfaces and save the assembly file.
Next time - Open file using last saved option.

Notes and References

9731605

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V220.0
Function: DISPLAY

Ref: 002-8510730

KB Article ID# PL8510730

Contents

SummaryDetails

Associated Components