Can I display to the "Drawing Views" the image that inserted to Sketch of Part?

2021-10-06T23:57:15Z

Summary


Details

Can I display to the "Drawing Views" the image that inserted to Sketch of Part?
Please advise how to do it or if there is any workaround.

Solution

As of now there is no direct option available in Solid Edge to show the image used in 3D part in its Drawing view in Draft. 
 
Currently we have only two possibilities:
- Map the image as a texture on a surface of the part, then generate a shaded view of the part in draft that can be used to accomplish this, but that would require modifying the part to have a face the desired size of the image.
Or
- To place the image in draft as an image object, constrain a corner to the corner of the sketch, then resize it to match the sketch rectangle.

Notes and References

9796170

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V220.0
Function: DISPLAY

Ref: 002-8510729

KB Article ID# PL8510729

Contents

SummaryDetails

Associated Components