Solid Edge Is there any feature available to place fasteners bill of material separately?

2021-10-06T23:57:15Z
DRAFT

Summary


Details

In an assembly drawing we would like to place separate fasteners bill of material just like we do for normal components. In the drawing we have an option available to place Parts list, hole table and tolerance table. So similarly is there any option/feature available to place fasteners parts list/bill of material separately?
 
Is there any solution/ workaround is available?

Solution

There is no direct option available to get parts lists separately of hardware used in the assembly.
 
As a workaround user can create a new assembly view configuration for hardware items only of an assembly and use the configuration to generate parts list.
While placing the parts list in the draft just ensure to deselect the 'Parts list - Link to Active' option.
 
In parts list the Configuration - Specifies an assembly display configuration to control what is displayed in the parts list. Selecting a predefined assembly configuration sets options for how subassemblies are treated in the parts list, what is included and excluded, what is shown or hidden. The default is No selection.

Notes and References

9812178

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V220.0
Function: TABLES

Ref: 002-8510727

KB Article ID# PL8510727

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS