Details
In NX go to:
1. Menu -> Preferences -> Selection.
2. Cursor (group) -> Show Cross hairs.
This setting was stored in NX 12 in the following registry key.
1. Registry Editor.
2. HKEY_CURRENT_USER -> Software -> Unigraphics Solutions -> NX -> <NX version> -> selection -> Crosshairs.
However, It is not there in the same location for 1899.
Where is this setting stored?
Solution
The "Show Cross hairs" setting is stored at below location.
C:\Users\(Username)\AppData\Local\Siemens\NX1899\UserPreferences.txt.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: xp64
Product: NX
Application: GATEWAY
Version: V1899
Function: PREFERENCES
Ref: 002-8510724