What is use of 'Associated with material' option from Gage Properties?

2021-10-06T23:57:13Z

Summary


Details

What is use of 'Associated with material' option from Gage Properties?

Solution

Associates the gage table with the material specified in the field. The button is enabled when the Use Excel File option is selected, a gage table is selected in the Use Gage Table, and a material is selected in the Material tab.


 When you select this option and click the Save button the gage table is associated with the material in the material library. Once associated in the material library, when the same material is applied to another file, the associated gage table is automatically used.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V220MP5
Function: OTHER

Ref: 002-8510720

KB Article ID# PL8510720

Contents

SummaryDetails

Associated Components