Details
Annotations falling outside the view break gap are being hidden on creation of view break.
Solution
For the annotations whose location falls outside the view boundary, like Intersection symbol etc, even though they do not fall inside the view break region, these annotations will be hidden, on applying view break.
The work-around for this issue is to:
1. Create these annotations inside the view boundary (in View Expand mode)
2. Edit the view boundary, change it to Manual and make the boundary large enough so that the annotation falls inside the boundary.
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1899
Function: DRAWING/VIEW
Ref: 002-8510591