Solid Edge When was Solid Edge certified to run on Windows 10?

2021-10-06T23:57:12Z
PART/SHEETMETAL

Summary


Details

Which was the first version of Solid Edge to be certified to run on Windows10?



Solution

Solid Edge ST8 MP3 was the first certified version to run on Windows 10.

See also "readme.htm" in the Solid Edge install folder for detailed specifications.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V104.0
Function: INSTALL

Ref: 001-9817046

KB Article ID# PL8509675

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES