Solid Edge List of NX Nastran commands to use in the command line for Solid Edge Simulation

2021-10-06T23:57:12Z
SIMULATION

Summary


Details

To set individual Nastran Parameters, you have the Nastran Command Line available from 'study/RMB/options'. 

Is there any list of NX Nastran command to use in the command line in Solid Edge Simulation?



Solution

If you have Femap or NX Nastran available you can check in the Help/Documentation for 'Installation and Operations Guide'.   The documentation can be found here:


  • C:/Program Files/Siemens/Femap 2021.1/nastranhelp/nxnastranhelp.htm
  • C:/Program Files/Siemens/Femap 2021.1/nastranhelp/pdf/install_guide.pdf
In Chapter 5 you will find 'Using the Basic functions of NX Nastran'. 

A full list of the valid keywords is given in appendix B of this document.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SIMULATION
Version: V221.0
Function: TOOLS

Ref: 001-8450817

KB Article ID# PL8509639

Contents

SummaryDetails

Associated Components

SIMULATION: ALL