Is there a way to specify a particular version of KeyShot to use with Solid Edge?
Solution
There is a registry key which specifies the active version of KeyShot. This is not specific to Solid Edge, so setting this will specify any startup of KeyShot will run the version specified in this key. The following text can be used to create a registry file. When that file is activated with the following text, Version 9 of KeyShot would become the active version. WARNING: This tip is only recommended for users who understand the risks of using registry files:
Windows Registry Editor Version 5.00
[HKEY_CURRENT_USER\Software\Luxion]
"KeyShotVersion"="KeyShot 9"
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V220MP5
Function: ERA
Ref: 001-9812729