Boundary selection - Incorrect Tool position on members

2021-10-06T23:27:43Z

Summary


Details

Changing the Tool position on multiple selected members of a boundary set only changes the setting on the first member. 
eg. shift select all of the members of a boundary set in the 'Part Boundaries' form and change the Tool Position setting to 'On'. The tool position 'On' is only set on the first member of the set. 



Solution

A workaround is to toggle the 'Tool Position' to 'Tanto', then toggle back to 'On' again. The 'On' setting will then be set on all of the members. 

This problem is fixed in NX 1899 series onwards 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1507
Product: NX
Application: CAM
Version: V1872
Function: BOUNDARIES

Ref: 001-9813723

KB Article ID# PL8509434

Contents

SummaryDetails

Associated Components