What information is required for a Solid Edge 2020 home use license?

2021-10-06T23:57:11Z

Summary


Details

What information is required for a Solid Edge 2020 home use license? 



Solution

You will need the Composite2 number that can be found on the License Utility once Solid Edge is installed. To access the License Utility, you can either attempt to run Solid Edge, which will give an error message and bring up the utility, or you can go to the Windows Start menu, select Siemens Solid Edge 2020 -> License Utility. This composite2 will then be used on the License Management webpage to generate a license file to run on your home computer.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1903
Product: SOLID_EDGE
Application: SETUP
Version: V220.0
Function: LICENSING

Ref: 001-9811739

KB Article ID# PL8509206

Contents

SummaryDetails

Associated Components