In this example a customer cannot borrow a license from their FlexLM License server, even though in the License of the Server the feature BORROW=xxxx can be found. The customer gets an error message,
indicating that a license has been detected with the command "USE_SERVER" and the borrow option is not enabled.
Solution
The reason for that message is that the Solid edge Client uses a License which has been generated automatically by starting the Solid Edge License Utility using the option 'I have a License Server name'.
Upon entering the Server name and clicking on OK, the existing license will be automatically replaced by a new one. This new license will not support license borrowing:
##############################################################################################
# Solid Edge Client License File
#Important: This license file will not support license borrowing.
# To support license borrowing you must have purchased floating licenses and
# you must replace this file with a copy of the license file on your license server.
##############################################################################################
SERVER machinename SE_HWKEY_ID=36243 27001
VENDOR selmd
USE_SERVER
Consequently, when then trying to borrow a license, the tool checks the license of the client and does not find the feature BORROW, but instead USE_SERVER.
The solution is, to copy the original Server License (containing the BORROW feature) manually to the client and to replace the above one (containing USE_SERVER) with the original. After this one can borrow a License from the License Server.
Notes
With the new Common Licensing tool , starting with Solid Edge 2020, this is no longer an issue, since this tool uses a System Variable called SE_LICENSE_SERVER, that points to the license to use. This Variable has always preference over the Solid Edge License File in the Preferences Folder of the client.
Notes
If you have further inquiries about floating Licensing please refer to the FAQs collection link below:
Solid Edge Floating License FAQs Collection