Mirror weldment assembly results in incorrect geometry

2021-10-06T23:57:10Z

Summary


Details

The customer has an assembly that is marked as a weldment.  When inserting it into a higher level and mirroring this assembly not all the geometry is mirrored correctly.  If the assembly is not a weldment assembly, everything is mirrored correctly.

The assembly to be mirrored appears like this within the parent assembly:

When mirroring the subassembly that contains the weldment features the result is as below:
Some components are moved from the correct position.

Solution


By editing into the subassembly it is observed that one of the assembly features is not updated (Mirror 3)

The first thing to do is to Recompute this feature.

Then return to the main assembly - Asm1.asm
Try again to create the Mirror component by selecting the subassembly  - now the result will be correct.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V219MP10
Function: ASSEMBLY
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V219MP9
Function: COMPONENTS

Ref: 002-8508771

KB Article ID# PL8508771

Contents

SummaryDetails

Associated Components