NX Windows 10 Update v2004 breaks NX1884, Simcenter 3D 2019.2 (v1884) and all prior releases

2021-10-07T00:09:01Z
NX Open NX for Manufacturing Licensing Teamcenter Share NX System Administration NX Design Translators NX for Design

Summary


Details

Update August 21, 2020:
2020-07 Cumulative Update for Windows 10 Version 2004 for x64-based Systems (KB4568831) contains the fix to the below-mentioned issue.

Jun 05, 2020:
The latest Windows 10 update v2004, released May 2020, has a bug that prevents NX1884, Simcenter 3D 2019.2 (v1884), and all prior releases from launching; this includes the interactive launch in native, managed mode as well as invoking any NX session using external custom NXOpen applications.  Currently, there is no known NX, or Simcenter fix that will resolve this issue.  We recommend that you do not update Windows 10 to v2004.

Our investigation shows that the bug is in the Windows update, specifically a bug in the universal C-runtime with the function strerror() in ucrtbase.dll.  We are working with Microsoft to fix this issue; we also recommend that you contact Microsoft if you have already updated Windows 10 to this release, or delay your Windows update to a release that has a fix for this issue.

Thank you in advance for your cooperation and understanding.  We will inform you when there is a fix available for this issue, until then our recommendation is to delay your Windows 10 v2004 update.  For more information please contact the Global Technical Access Center in your local region, or area.



SFB-NX-8508209
Product Information:
  • Product: NX
  • Product: Simcenter

KB Article ID# PL8508209

Contents

SummaryDetails

Associated Components

Block/UI Interface Stylers Knowledge Fusion Menuscript NX Open - All Languages NX Open Python Open for C/C++ Open for CAE Open for GRIP Open for Java Pre-NX6 UI Styler SNAP UDO