Points in a drawing Print / Plot are much larger compared to their display in the work area

2021-10-06T23:27:42Z

Summary


Details

 Points displayed on the drawing are much larger than shown in the work area when plotted or printed.

Solution

In the Menu, select 'Preferences-->Visualization'. Expand 'Color' and highlight 'Handles'. On the right under Handle Settings, set the Handle/Point Size to 'Small'.  OK.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V1847
Function: DRAWING/VIEW

Ref: 002-8508129

KB Article ID# PL8508129

Contents

SummaryDetails

Associated Components