Which version of Solid Edge is compatible with NX 1884?
Solution
Please check the following sections of the "readme.htm":
"Parasolid Versions for Solid Edge "
"Solid Edge, Femap, and NX plmxml"For Solid Edge 2021 file compatibility with the latest releases of NX and Femap, the latest plmxml adapter may be needed and will be available after the Solid Edge 2021 release at:
https://download.industrysoftware.automation.siemens.comSelect Solid Edge→Product updates→2021→PLMXML.
For NX, the adapter should be copied to the NX installation folder, %UGII_BASE_DIR%\NXBIN.
-------------------------------------
For a direct open, the Parasolid versions need to be the same or newer in Solid Edge.
The regular solution to overcome the versioning is to download the plmxml-adapter as described above.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V221.0
Function: NX
Ref: 001-9792154