Part family members are not getting cloned

2021-10-06T23:27:42Z

Summary


Details

The cloned assembly is treating the members as lost

Solution

Set the following variable and restart NX:

UGII_UGMGR_ALLOW_PFM_IMPORT_EXPORT = 1

Used for family members with no templates when importing and exporting assemblies. 

If the variable is not set then the family members will not be imported into portal. 

If the variable is set, then it will be given precedence over UGMGR_CloneImportExportAutoRemovePFM. 

When an assembly referencing part family members is imported/exported, there will not be any change to the existing behavior. The required part family members will be automatically generated during this process.





Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V1847
Function: ASSEMBLY_MODEL

Ref: 002-8507824

KB Article ID# PL8507824

Contents

SummaryDetails

Associated Components