Details
When a part having PMI section views is imported into an another part, PMI's associated to the PMI section view curves, are retained.(lost associativity of it's references)
Solution
Inter part copy/paste of PMI section views, is not supported currently.
So the PMI's associated to all the PMI section view curves, will be retained.
So as a work-around, user has to re-generate the PMI section view curves and has to re-associate all the retained PMI's to these new section view curves.
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: PMI
Version: V1867.4700
Function: SECTION_VIEW
Ref: 002-8507780