Details
In case of a out of sync assembly, Export operation uses which structure, NX or the TC structure?
Solution
By default, NX structure will be used to export the assembly outside teamcenter.
For the out of sync assemblies, having different TC and NX structures, NX structure will be used for the export operation.
So user has to sync the TC structure to the NX structure to export the assembly correctly.
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: CLONE_EXPORT
Ref: 002-8507779