Details
Some components are added as Reference Only components in the non master drawing file.
These components are not present in the master file structure.
These components will get added in the non-master drawing file as reference only components, when the user creates views selecting explicitly only these components.
So when user exports this assembly outside Teamcenter by specifying the Master item, these non-master specific components are not exported.
Only components in the master structure are exported.
Solution
In this case, as master and non-master items have different structures, exporting master item, will only export the components associated to master structure and it's related non-master files.
The components which are added as reference only in the non-master drawing, are not exported.
So to export the non-master drawing specific components, explicitly specify the non-master dataset in the export operation.
Like "@DB/61214373-80/1/specification/61214373-80-1-dwg".
This will export all the components associated to the above non-master drawing file.
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1899
Function: CLONE_EXPORT
Ref: 002-8507778