Cross Tenancy

2020-06-02T02:13:08Z

Summary


Details

You want to share asset data between tenants and need to learn more about MindSphere's Cross tenancy feature.

Solution

  1. Can we share both physical and virtual assets?

  2. When assets are shared, will the time-series data of developer tenant assets available in an IOT value plan tenant?

    • Yes

    • If the time-series data is available in an IOT value plan Tenant, is it possible to read that data using time-series API?

      • Yes,only read is possible.

      • In Restrictions it is mentioned that shared types/aspects cannot be edited or deleted and core.sharerenterprise assets cannot be updated.  So once an asset is shared if we cannot edit and we need to add new data point, what should we do?

        • The shared Asset itself will have the same type as on the other tenant. So you can update it as you wish BUT only on the tenant where it's shared from.

        • Notes

          KB Article ID# PL8507609

          Contents

          SummaryDetails

          Associated Components