EXCEPTION: Error code 3070008 seen in ugs_router log while launching NX

2021-10-06T23:27:41Z

Summary


Details

Received below error in ugs_router log while launching NX (1899) from TC (12.3).
-----------------------------
NTEROP: Establishing client-proxy for interoperating


INTEROP: Attempting to interoperate with UG/Manager V1899 1...


INTEROP: Waiting for Mutex: UGS Mutex UG/Manager V1899 1


INTEROP: Obtained Mutex


INTEROP: Releasing Mutex


*** EXCEPTION: Error code 3070008 in line 605 of o:\nx1899\ip1700\src\interop\no\ind\interop_socket_writer_definitions.c at Fri May 22 11:13:53 2020 India Standard Time


+++ Failed to connect to port 49873 on localhost
-------------------------------


Solution

"Running Applications" registry entry had a left-over value for NX1899, so ugs_router was trying to attach to that and failing. 

Delete the value under
HKEY_CURRENT_USER\Software\Unigraphics Solutions\Running Applications
Solved it.

Notes and References

9783634

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1899
Function: STARTUP

Ref: 002-8507243

KB Article ID# PL8507243

Contents

SummaryDetails

Associated Components