NX
How to use Euler Angles in CMM 5 axis positioning probing head ?
2021-10-06T23:27:41Z
NX for Manufacturing
Summary
Details
Would like to set probing operation under the measured coordinate system, which is not compatible with the machine system.
The probing head is oriented by the angles in degrees and would like to output the head angles in Euler angles which is corresponding to the measured coordinate system.
This is very useful thing to measure feature under local coordinate system because the head has a limit angle so Euler Angles will solve that.
Solution
The user needs to enable the Euler angles using a special command.
Hardware/Software Configuration
Platform: all OS: n/a OS Version: n/a Product: NX Application: CMM_INSPECTION Version: V1915 Function: OTHER