Tecnomatix RobotExpert Controllers for KAWASAKI, KUKA

2021-10-07T00:11:32Z
Virtual Reality Intosite Process Designer Dimensional Planning Validation Teamcenter Share Process Simulate Web-Based BOP Manager [eMS Platform] eM-Server

Summary


Details


Dear Siemens PLM Software Customer, 

We are pleased to inform you that RobotExpert controllers for "KAWASAKI, KUKA" 
are available for download from https://download.industrysoftware.automation.siemens.com. 
 
See RobotExpert_Controller_Name_changes_log.htm for details 
concerning this update. 

Note: This file is located in the 'Change_Logs' folder directly 
           under the 'Robot_Controllers' folder. 
 
 
Use the following steps to download. 
 
Note: A valid WebKey account is required. 
(URL: https://plmapps.industrysoftware.automation.siemens.com/webkey/) 
 
In your browser address window enter the URL: https://download.industrysoftware.automation.siemens.com/ 
 
WebKey Username: [your WebKey user ID] 
 
WebKey Password: [your WebKey password] 
 
Select the Download tab 
 
In the Product Filter area scroll down to Tecnomatix Products 
Select Tecnomatix Products 
Expand Product updates 
Expand RobotExpert/ 
Expand Robot_Controllers/ 
Expand V11.1/, V12.1/, V13.0/, V13.0.1/, V13.0.2/, V13.1/, V13.1.1/, V13.1.2/ or V14.0/ 
Expand KAWASAKI or KUKA 
 
Download the file(s): 
 
    RobotExpert_11.1_KAWASAKI_AS_32BIT_v2.35_12_10_2017.exe 
    RobotExpert_11.1_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_11.1_KAWASAKI_AS_32BIT_v2.35_12_10_2017.exe 
    RobotExpert_11.1_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_11.1_KUKA_KRC_32BIT_v3.44.2_12_10_2017.exe 
    RobotExpert_11.1_KUKA_KRC_64BIT_v3.44.2_12_10_2017.exe 
 
    RobotExpert_12.1_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_12.1_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_12.1_KUKA_KRC_64BIT_v3.44.2_12_10_2017.exe 
 
    RobotExpert_13.0_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.0_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.0_KUKA_KRC_64BIT_v3.44.2_12_10_2017.exe 
 
    RobotExpert_13.0.1_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.0.1_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.0.1_KUKA_KRC_64BIT_v3.44.2_12_10_2017.exe 
 
    RobotExpert_13.0.2_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.0.2_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.0.2_KUKA_KRC_64BIT_v3.44.2_12_10_2017.exe 
 
    RobotExpert_13.1_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.1_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.1_KUKA_KRC_64BIT_v3.44.2_12_10_2017.exe 
 
    RobotExpert_13.1.1_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.1.1_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.1.1_KUKA_KRC_64BIT_v3.44.2_12_10_2017.exe 
 
    RobotExpert_13.1.2_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.1.2_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_13.1.2_KUKA_KRC_64BIT_v3.44.2_12_10_2017.exe 
 
    RobotExpert_14.0_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_14.0_KAWASAKI_AS_64BIT_v2.35_12_10_2017.exe 
    RobotExpert_14.0_KUKA_KRC_64BIT_v3.44.2_12_10_2017.exe 
 
 
To Install: 
 
Place RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe 
into a folder ($Tecnomatix/downloads is suggested). 

Run RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe. 

Where $Tecnomatix is the full path to the RobotExpert installation. 

The default installation point is C:\Program Files\Tecnomatix. 
 
 
If you have any issues with the installation or support of these fixes, 
please contact your local GTAC support group. 
 

Sincerely, 
 
Siemens PLM Software 



SFB-TECNOMATIX-8001090
Product Information:
  • Product: TECNOMATIX

KB Article ID# PL8001090

Contents

SummaryDetails

Associated Components

VR Analyze