NX
Incorrect journal created when using Feed Rates functionality
2021-10-06T23:27:40Z
NX for Manufacturing
Summary
Details
When recording a journal and using the Feed Rates functionality (in the Operations group on the Ribbon Bar), the journal will contain entries like this:
// can not output code to find <JABL>: <UGS::CamBuilder::InheritableExtendFeed> &00007FF4127EAD90 [82272] NXOpen.CAM.InheritableFeedBuilder nullNXOpen_CAM_InheritableFeedBuilder = null; nullNXOpen_CAM_InheritableFeedBuilder.Value = 90.0;
This will cause the journal to fail when played back. How can we edit the feed rates of an operation using a journal?
Solution
When recording a journal we can see that the Feed Rates option does not have a small green square. This means that the functionality is not journaled.
The solution is to instead edit the operation and change the feeds and speeds within the operation. Then the system will be able to record the journal with the correct builder.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: CAM Version: V1899 Function: JOURNALING