EXCEPTION error when opening files

2021-10-06T23:27:40Z

Summary


Details

Part file could not be opened because foreign expression detected.

Syslog shows:
+++ Invalid foreign expression

Solution

A partial work around exists for this corruption.

Set the environment variable UGII_KF_CLEANUP_IPE_ON_LOAD=1 and then open the corrupted file. 
This will remove the interpart references in the file, so usage should be limited, but it will allow you to retrieve some of the file data.

Notes and References

EXCEPTION: Error code 1050023 in line 741

 +++ Invalid foreign expression.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1899
Function: EXPRESSION

Ref: 002-8506622

KB Article ID# PL8506622

Contents

SummaryDetails

Associated Components