NX UGCLONE cmd to output prt file without _rev

2021-10-06T23:27:40Z
NX for Design

Summary


Details

How to run the ugmanager_clone command line utility to export NX data to OS without revision appended to the OS filename?


Example: 
When exporting out the following Teamcenter item revision: 000160/A to OS using ugmanager_clone, the default resulting OS file is named 000160_A.prt; how to have it export out without the revision append to the OS file name like 000160.prt?



Solution

In the command window prior to running the script, set the following environment variable first:
UGII_UGMGR_ITEMID_IS_OSFILE_NAME=yes



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V11.0
Function: CLONE

Ref: 001-9774703

KB Article ID# PL8506560

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX