Solid Edge How to map the Material Thickness (Gage) to Teamcenter?

2021-10-06T23:57:08Z
DOC_MANAGEMENT

Summary


Details

The customer is able to map the Solid Edge Material property to Teamcenter, but how can they map the Sheet Metal Material Thickness to Teamcenter?  

Solution

In Solid Edge we are able to map exposed variables to Teamcenter.  In this case the Material Thickness is an existing property in the variable table and by default the property is already exposed.

 

Map this attribute to a custom property created in Teamcenter so that it is similar to example shown below:

Now both the Material and Material Thickness will be synchronized in the Common Properties Dialog:







Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC

Ref: 002-8506546

KB Article ID# PL8506546

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC