Deselect All Colors option for Visible Lines not available in NX1899+
2021-10-06T23:27:40Z
Summary
Details
After placing a view on the drawing, the drawing view geometry is not the same color as the model geometry. Prior to NX1899 this could be resolved with the following procedure: 1. Highlight the drawing view boundary and select 'Settings'. 2. Expand 'Common' and highlight 'Visible Lines'. 3. Select the color Icon under Format on the right.4. On the color palette select the 'Deselect All Colors' option. 5. OK out of the menu. The drawing view geometry will now be the same as the model geometry.
In NX1899+ there is no 'Deselect All Colors' option.
Solution
In NX1899+, the new color palette is shown below:There are two workaround to 'Deselect All Colors'. Workaround 1: On the color palette above enter zero "0" in the 'Find' field. Hit <enter>. OK out of the dialog.
Workaround 2: Once the color palette appears, press the Ctrl key on the keyboard and select the color twice which is already selected. This will result in color deselection. OK. Development confirms this is resolved in NX1926, per PR #8445041.
Hardware/Software Configuration
Platform: all OS: n/a OS Version: n/a Product: NX Application: DRAFTING Version: V1899 Function: SETTINGS