Solid Edge How to add a characteristic value of a Standard Part already extended.

2021-10-06T23:57:08Z
APPLICATION

Summary


Details

Added a material characteristic to a Standard Part with two values using 'Extend Existing'. A new requirement called for a third material to be added to the list of values.

Solution

Use the 'Extend Existing' command on the original Standard Parts that were extended. It gets you back to the dialog for the variable extended where you can add new values. In this case, a third material.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: APPLICATION
Version: V219MP11
Function: STANDARD_PARTS

Ref: 002-8431897

KB Article ID# PL8431897

Contents

SummaryDetails

Associated Components

APPLICATION: STANDARD_PARTS