NX PMI dimension reposition not updating on the drawing view

2021-10-06T23:27:40Z
NX for Design

Summary


Details

PMI dimension location in the drawing is not updating to the new location of the PMI in modeling.



Solution

For standard PMI dimensions in modeling to have their location the same as the drawing view and have them update in the drawing view if their position is changed in modeling, the Inherit PMI Tracking option 'Annotation Location' must be enabled, which can be set in the drafting application Menu -> Format -> Inherit PMI Tracking. 


Note: Currently, there is no default setting source, but the "inherit" XML Document found in C:\Program Files\Siemens\NX1899\UGII\pmi\property can be modified by changing the text from "none" to "track" for AnnotationLocation and saved. Restart NX for this to take effect. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: xp64
Product: NX
Application: PMI
Version: V1899
Function: INHERIT_TO_DRAW

Ref: 001-9765651

KB Article ID# PL8412041

Contents

SummaryDetails

Associated Components

PMI