Solid Edge Unlocked Rotation of automatically placed flanges in Solid Edge Modular Plant Design

2021-10-06T23:57:07Z
PART/SHEETMETAL

Summary


Details

The Customer is using Modular Plant Design.  When they generate a pipeline, the flanges on the Pipeline are under-constrained. The Customer wants them to be completely constrained.


Is there an option so that Piping Design places the Flanges completely constrained? 



Solution

In the Modular Plant Design (MPD) setting there is an option to lock the end components.  When this option is checked, the end component gets locked on the axial constraint independently of other components. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: SE_PLANT_DESIGN
Version: V220.0
Function: P&ID

Ref: 001-9758549

KB Article ID# PL8372908

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES