Which licenses do I need to borrow when using the Licensing Tool?
When borrowing licenses, the available licenses in the Borrowing Settings are
not the same as the available bundles in the Bundle Settings.
Each INCREMENT on the license file has a user_info field.
This user_info is shown in the Licensing Tool for both the Bundle Settings and
the Borrowing Settings.
The Bundle Settings only shows the Packaged license Bundles on the license
file.
The Borrowing Settings shows all license INCREMENTS that can be borrowed.
In some cases license features are not Packaged but floating license features
on the license file. These will be listed in the Borrowing Settings but not in
the Bundle Settings.
It is possible to rename the user_info field on the license file. Please refer
to the Editable Parameters of the License File section of the SPLMLicensing
User Guide.