The need of editing multiple parameters for several CAM operations
Solution
There is a feature named
"Mass Edit", available from NX1899 that needs to be activated manually under
File-->Utilities-->Feature Toggles (Toggle expires in NX1926)
Find
MfgCore_MassEdit and activate it by setting
"On" State
After the activation, note that this particular toogle doesn't need a restart, if you select multiple operations in your Operation Navigator, you have the
"Mass Edit" option available, so you can edit multiple operations parameters at the same time.
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1899
Function: OPERATION
Ref: 002-8333187