How to break the associativity of a balloon callout from the parts list

2021-10-06T23:27:39Z

Summary


Details

How to break the associativity of a balloon callout from the parts list, so that text can be edited/modified and will not update according to the parts list.



Solution

1. With the Balloon dialog open, select the 'Select Terminating Object' option under the Leader group of the dialog.
2. Turn off the 'Enable Snap Point' option in the slim ribbon bar.
3. Place your cursor at the desired location and place the balloon (it may be needed to zoom in on the area).
4. The balloon is not associated to anything, and the text can now be edited and will not update with the parts list.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V12.0.2
Function: ANNOTATION

Ref: 001-9759501

KB Article ID# PL8173495

Contents

SummaryDetails

Associated Components