Unable to find PMI Effectivity in Preference - PMI
Solution
Ensure File - PMI is enabled.
Now you would see additional PMI related options as shown below(Still PMI Effectivity is missing) :
Ensure you have set ON the customer default as shown below for "Infer PMI Effectivity":
Now you would see PMI Effectivity :
Note:
If you are still not able to see Effectivity option that means you have opened Single piece part.
Ensure you have opened an Assembly then you should see this "Effectivity" option.
Notes and References
8979393
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: PMI
Version: V1847
Function: EFFECTIVITY
Ref: 002-8171822