Details
Getting 'LoadLibrary Failed with error 87' when starting Solid Edge via Remote Desktop.
Solution
This is initially documented at the following URL:
https://superuser.com/questions/1516486/windows-10-loadlibrary-failed-with-error-87-on-remote-desktop-session
Remote Desktop may not interact well with graphics and you have to change the way that the workstation at the office is being accessed.
Notes and References
IR#9744550
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: APPLICATION
Version: V220.0
Function: OTHER
Ref: 001-9749940